We Built Our Reputation On Reliability
Everybody knows the money stops as soon as your generator does. That’s why for the last 100 years, we’ve built some of the best commercial generators on water. Every weld, wire and circuit is a badge of honor. If our craftsmen have touched it, it is good and true. And if our name is on it, it’s going to work. From handcrafted alternators to hand-built controllers, we take pride in building power systems you can depend on.
The First and Only Built-In Paralleling System
We created the first marine generators with built-in paralleling controllers. Our PGEN connection parallels up to eight Rehlko generators of varying sizes with a single communication wire. When the first generator’s load is light, the second generator automatically drops off. When the load is heavy, the second generator automatically comes online to provide the power needed to carry the load.


Bottom Line. It's All About Your Bottom Line
We created the Decision-Maker® 3500 controller to eliminate the need for expensive, oversized switchgear, costly add-ons and complicated installations. Not only that, our new controllers feature auto-transfer functionality. If one generator is in trouble, the second generator senses the problem, starts up and takes on the load— automatically. So your boat will never be dead in the water. And you can keep your business in business.